Tool/software:
Hello everyone:
If any of the outputs of U12, U13, or U14 fails, the audio circuit will fail (no audio output).
This typically occurs after about four hours of device burn-in.
When this happens, the op amp becomes hot, and the impedance measured between pins 8 and 4 is only 275 ohms. (typically 8.5 megohms)
I don't understand what's wrong with this circuit design. I haven't measured any abnormal voltages or inrush current at the op amp inputs or outputs. Is this MC33078 not suitable for use with the DAC(AK4458)?
Can anyone help me?2451.DAC.pdf