This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM2900C: PCM2900C technical inquiry

Part Number: PCM2900C

Tool/software:

Dear All,

Our company want to develop an AUX-USB device, trying to review by PCM2900C.

Got two question for the item as below.

1. Checking on the datasheet it appears to operate hardware-base, without separate firmware. Is this correct? 

    If firmware is required, please help to check how to configure the development environment.

2.
What version of UAC (USB Audio Class) is supported? (It is expected to be 1.0, as it looks only supports USB Full-Speed.)
If not, please let me know.




Thank you.
  • Hi Jongsoon,

    1) No firmware is required. The device leaves the factory class compatible with USB1.1

    2) USB is backwards compatible, so it will work on USB 2.0 or 3.0 systems, but only USB 1.1 features are available.

    Best regards,
    Jeff McPherson