This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320DAC3101: Application issues.

Expert 2340 points

Part Number: TLV320DAC3101

Tool/software:

Hi Team,

Use TLV320DAC3101IRHBT ,

Currently, the usage (as shown in the figure below) of the left and right channels of the DAC is equivalent to connecting four power amplifiers. It needs to be confirmed whether this usage is feasible? Or do you have any recommended solutions?

 AUDIO-XMOS-V20-250928-0930.pdf

  • Hello,

    On our EVMs we often use xmos or TAS1020 IC with our dacs and amplifiers , so  the above  is feasible.  The SPK output pins need a load of 8 Ohm Min and the HP pins a min load of 16 Ohm. You can always refer to users guide in the product page for the schematic reference.

    I  would add 22 to 100 Ohm series resistors on I2S signals and ground any unused analog input pin via a cap.

    if  your interested you can also refer to   SLVA689–February 2015    I2C Bus Pullup Resistor Calculation 

    Regards,

    Arash