Other Parts Discussed in Thread: OPA1632,
Tool/software:
I want to use the OPA1633 or OPA1632 to buffer an ADC input. What is the proper way to protect the ADC input from overvoltage? My chosen ADC has absolute analog input ratings of -0.3 to 3.6V. I thought about clamping both of the differential signal lines before the OPA1633 to half the maximum voltage range to about ±1.6V, but if I have a single-ended input that would only allow half the full scale ADC range to be used. What's the best approach here?