I'm trying to choose between PCM2900C and PCM2904, but I can not fully understand how these devices differ. The other pretender is PCM2901. Is the low voltage supply only difference between it and PCM2900C&PCM2904?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Alex,
The PCM2900C is compatible with Windows 7 and compliant with USB 2.0. The application note below details all the changes between the PCM2900B and PCM2900C. The PCM2904 is similar to PCM2900B so, some of the big differences should be similar to the improvements made in the C revision. What is your application and main concerns about each part?
http://www.ti.com/lit/an/sbfa020/sbfa020.pdf
Regards,
Michael Green