Part Number: TLV320AIC3254
Other Parts Discussed in Thread: TAC5212
Dear Team,
We are planning to use the TLV320AIC3254 device in our design. We had initially selected this part because it featured Acoustic Echo Cancellation (AEC) and Active Noise Cancellation (ANC) capabilities. However, in the latest datasheet, these features have been removed. Could you please clarify the reason for this change?
(Note: “Deleted ‘Acoustic Echo Cancellation (AEC)’ and ‘Active Noise Cancellation (ANC)’ from applications list” is mentioned in the revision history.)
Our requirement is to support two microphones and two 4 ohm, 3 W speakers using the built-in audio amplifier. The device should also support active noise cancellation, and it would be preferable if there is a pin-compatible alternative available in space-grade quality.
Please suggest a suitable device that meets these requirements.
With Regards,
Yashash