TAD5212: Inquiry about allowable BCLK/FSYNC ratio tolerance for TAD5212

Guru 12530 points
Part Number: TAD5212


Hi,

We are currently evaluating the TAD5212 in our audio system design and have a question regarding the clock error detection and BCLK/FSYNC ratio tolerance.

In the datasheet, we could not find explicit information about the allowable deviation range (tolerance) of the BCLK-to-FSYNC ratio before the device reports a clock error or fails to detect the sampling rate correctly.

Could you please clarify the following points?

  1. What is the allowable tolerance (in %) of the BCLK/FSYNC ratio for the device to operate without a clock error?

  2. Does this tolerance depend on the “Auto sample rate detection mode” or the register setting (PASI_FS_RATE_NO_LIM @ 0x32)?

  3. Are there any internal registers or status flags that indicate when the ratio is out of range?

Thank you very much for your support.
Best regards,

Conor