Part Number: OPA1611
Other Parts Discussed in Thread: TINA-TI
Hello, I want to build a preamplifier with an input impedance of 5 kohm. The signal I need to measure is a 200 nVrms signal at 30 kHz. First, I wanted to take this signal with a low-pass filter with fc = 40 kHz. However, since my bandwidth is very wide (I took my noise bandwidth as 64 kHz), even if I use an op-amp with the lowest input voltage noise density (e.g., OPA1611), only the op-amp noise alone becomes 278 nVrms due to en*sqrt(64000). And because of the Gaussian distribution, the peak value of this noise becomes 278n * 6.6 = 1836 nVpp, which means that the real signal we need to measure will disappear inside the noise. I think the only area I can adjust to reduce the op-amp’s input noise is the feedback path. Since I don’t have much knowledge about bandpass preamplifiers, I couldn’t make progress. I need your support on this. Is there anything wrong in my way of thinking? What are your suggestions?