I have a question regarding the use of this device in 3-Wire PCM mode with the LRCK sample rates listed in Table 11.
Due to hardware variations and ambient temperature effects, the supplied sample rate frequency may deviate from the target value. Could you please let us know the allowable percentage deviation in the LRCK sample rate frequencies listed in Table 11 within which the device will operate normally?
In particular, we would appreciate it if you could provide the allowable deviation for the 16 kHz and 32 kHz sampling rates over the full temperature range of -40 to 130°C.