This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3254EVM-K: miniDSP program

Part Number: TLV320AIC3254EVM-K
Other Parts Discussed in Thread: TLV320AIC3254, TLV320AIC3204

I wanted to know if miniDSP present in TLV320AIC3254 IC is programmed when we receive the product from TI or do we need to program the miniDSP again. I wanted to know this because when I try to route inputs in TLV320AIC3204_54_RHB_EVM to line outputs, I am unable route it through ADC & DACs(digital routing).

  • Hi Gauthami,

    You will need to load the algorithms and program the miniDSP after you power up the device.

    Best,

    Garret

  • Where can i find the "PurePath Studio Portable Audio Device App for TLV320AIC3254". I have installed  the PPS core (portable audio) 5.95, but require the .ppxml and app folder for TLV320AIC3254 miniDSP, and can’t find it on the product page and the installed folder.

  • Basically I need to route INI1_L to LOL through ADC/DAC. If we need to program the miniDSP then I need a pass-through.bin file for basic ADC-DAC connection. How will I be able to do that?

  • Hi Gauthami,

    I am going to reassign this thread for better support.

    Best,

    Garret

  • Hi,

    The portable audio version of PPS should have the AIC3254 framework already installed. When you open up PPS, go to Frameworks and then you should see "AIC3254", like this:

    However, if you just want to do a bypass from IN1L to LOL, the AIC3254 has an analog bypass mode through the mixer amplifiers where you can do this without any miniDSP/PPS, just register writes. The path would look like this:

    I would recommend this way over using PPS if you are just trying to do an analog bypass. If you wanted to do more complicated internal routing or extra processing, then you can use PPS. 

    Let me know which you prefer and I can help more with specific scripts.

    Best,
    Mir

  • Hi, 
    I was able to perform analog bypass mode to route IN1_L to LOL but I would like to route it through ADC/DAC as well. Can i dump the miniDSP program into IC without using PPS. whether miniDSP program readily available which will help me in routing IN1_L to LOL. I just want basic routing. I do not want to perform any complex function. All i want is to route it using ADC/DAC which required miniDSP program.

  • Hi,

    I see. Unfortunately we need to use PPS to generate the code that programs the miniDSP. However once that code exists, you can run it like any other I2C command. 

    What is your current I2C script? We need it to include in PPS. I can help you with creating the file but I would need all input/output settings. You put the I2C commands you are already using for routing and such in the SystemSettingsCode part of PPS. The input/output config in the GUI would look like this for a generic analog input to a generic analog output, then in the SystemSettingsCode part, we set which input and output it uses: 

    Again, what settings do you need for ADC/DAC with miniDSP that do not work with analog bypass mode? If you just wanted to route ADC to DAC without using miniDSP, you can also use a jumper between DOUT and DIN, doing a physical digital bypass.

    Best,
    Mir

  • Hi mir, 

    I do not have any working I2C script other than the analog bypass mode using analog mixers. Is it possible to discuss this over a call (Probably next week) depending on your availability? I need support for using the software to dump miniDSP. Also, I want to know about how I can use this evaluation kit for my application. 

  • Hi,

    Sure, I will send you a friend request so we can discuss via email.

    -Mir