This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAA5412-Q1: ESD issue

Part Number: TAA5412-Q1

Hi team,

The customer needs to perform ESD tests at ±2kV, ±4kV and ±6kV, but the ESD rating of TAA5412-Q1 is ±2kV. They are using a 100V/110nF capacitor as an ESD discharge device in MIC1+. Can this design withstand direct electrostatic discharge of ±6kV? If not, do you have any recommended solutions?

BR,

Jade