Part Number: LM4562
Hello,
a customer ordered 10 of the LM4562NA/NOPB at Mouser and came back with the following:
"In my design, I took into account the fact that at a voltage of +/-15 V,
the power supply load is typically 10 mA and a maximum of 12 mA. This is
in line with the specifications. However, I am measuring between 14 and 16
mA. How is this possible?
"The operational amplifiers were mounted as followers in a circuit at room
temperature. The output and negative input were connected, and the
positive input was connected to ground via a 1 Mohm resistor. This allowed
me to measure the offset, which is in line with the specifications. The
power supply, a laboratory power supply, has a 100 ohm resistor on the +15
V connection, which allows me to measure the supply current. I also
performed this measurement with an ammeter, obtaining the same result:
14-16 mA. I use 10 of these operational amplifiers in my circuit, and if
they consume more than expected, I will have to adjust the power supply."
Can you advise?
Thank you,