Part Number: PUREPATHSTUDIO
Other Parts Discussed in Thread: TAS2781
To Texas Instruments Audio Team,
I am a hardware engineer developing a product using the TAS2781. I am currently conducting a stress test where I need to force a continuous 4V sine wave output to the speaker.
I understand from the "Smart Amp Tuning Guide" that I must use ROM Mode to truly bypass the Smart Amp protection algorithms. And I have the following questions to clarify how to achieve a "protection-free" state:
1. When I switch the device to ROM Mode via PPC3 (Device Control panel), are the Excursion and Thermal Protection algorithms automatically disabled? Or do I need to manually write to specific registers to disable them even in ROM Mode?
2. I am using a DC power supply for this test, not a battery. In this case, Brown Out Protection (BOP) could affect the result? if then, Could you please provide the specific Register Address and Bit settings to completely disable the BOP feature?
3. Other Hardware Limiters Besides Smart Amp protection and BOP, are there any other internal limiters (e.g., Peak Voltage Limiter, Hard Limiter) enabled by default in ROM Mode? If so, how can I disable them?
4. Recommended Sequence My goal is to bypass ALL protections and force the amplifier to output the input signal as-is (pure 4V output) on my custom board. Could you recommend the correct register configuration sequence to achieve this?