Part Number: TAC5112
Hi team,
- Does TI provide an official Linux driver in which the TAC5112 GPIO pins (GPIO1, GPIO2, etc.) can be configured and used explicitly as general‑purpose GPIOs (GPI/GPO) under the standard Linux GPIO framework (e.g., sysfs or libgpiod)?
- If such a GPIO-capable driver (or patches) exists, could you provide it or share the download link?
- If this is not currently available, would it be possible for TI to provide an updated driver or guidance (for example, device tree examples and register settings) to enable general‑purpose GPIO control on TAC5112 under Linux?
Best Regards,
Ryu.