This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM5310 Datasheet

(Register 13, headphone short-circuit protection enable/disable), bit 5 is shown to be SHCR and bit 1 is shown to be SHCL. The function of SHCR/SHCL is not listed anywhere in the documentation.  What is the function?

Page 45, SRCR & SRCL - Reset Short-Circuit Protection for Headphone

 The description says "These bits initialize the short-circuit protection for the headphone outputs by setting SRCR = SRCL = '1'. After completing the initialization, the data of both registers are automatically set to '1'." The box showing different settings for these bits says write 0 to  these bits to activate reset, after which the bits are automatically set to 1. Also, the way the description is worded, specifically the "SRCR = SRCL = '1'" part, makes it sound like both of these bits have to be simultaneously written. Is this true or can each channel be reset independently?