Part Number: TPA3221
Other Parts Discussed in Thread: TPA3255
Hi team,
I have a question about TPA3255.
When MODE pins are set to M1=0, M2=1 for PBTL mode, I need to ground audio inputs INPUT C and D (pins 16, 17).
Should the grounding be done mechanically using jumper pins like on the evaluation board, or can it be done electrically using FETs or transistors?
Also, the datasheet states that PBTL output becomes mono BTL when INPUT C (pin 16) is at HIGH level with DVDD voltage. What is the voltage threshold for this? Is it the same as VoH and VoL specified in section 7.5 STATIC DIGITAL SPECIFICATIONS?
Best regards,
Kazuki Itoh