This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Testing SGI EVM



Dear All:

I just purchased a TI SGI EVM board.  I am trying to setup the environment to test the board.  When I ran the Metrology Demo with AIC3106 connected (S2:2 is off), the SPE EVM Demo program on PC showed some random readings.

When the AIC34 is connected (S2:2 is on), the SPE EVM Demo program on PC showed zeros on all readings.   Even I connected the AC (110V) to the input E, the values on the display remained the same (i.e, all zeros).  

Do I need to do anything in order to make the demo work?

Thanks

Best Regards

Men-Shen