Part Number: AM620-Q1
Other Parts Discussed in Thread: SYSCONFIG
Also, if there are any known limitations or constraints when applying SMP to real-time audio use cases, I would like to understand them.
Satoshi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM620-Q1
Other Parts Discussed in Thread: SYSCONFIG
Hi Satoshi,
Thank you for your query. I will check with the team internally about the plans for creating this document or if some document is already present. Kindly expect a reply in a couple of days.
Regards,
Ritapravo
Hi Ritapravo,
Thanks for checking.
I'll wait for your update .
Best Regards,
Satoshi
Hi Ritapravo,
Additionally, I am aware of the following example as well, although I understand it is primarily for reference:
Best regards,
Satoshi
Hi Satoshi-san,
Thank you for your patience and apologies for the delay. We are actively working on the SMP guide creation and is going through a series of checks before being available. Please wait for 2/3 days before we can provide it to you.
Regards,
Ritapravo
Hi Satoshi-san,
Please review the attached SMP guide. We hope it addresses all your queries comprehensively.
Please let us know if you require any additional assistance.
Regards,
Anil.
Hi Anil-san,
Thank you for sharing the SMP guide. It is very helpful.
I have a couple of follow-up questions after reviewing the document.
First, I would like to confirm on which A53 core the McASP interrupt and its completion callback are executed.
Even if the McASP initialization is performed on Core 0, is there still a possibility that the interrupt/callback could be handled on other cores?
Secondly, I would like to clarify a concern regarding core placement.
If the callback is executed on a different core (e.g., Core 1), while the audio processing task is pinned to Core 0, it seems that buffer/data transfer across cores would be required.
In such a case, I assume that additional latency may be introduced due to cross-core communication.
Based on this, I am assuming that it may be necessary to place both the interrupt/callback handling and the audio processing tasks on the same core.
Could you please confirm whether this understanding is correct, and if there is any recommended approach for handling this in FreeRTOS SMP?
Regards,
Satoshi
Hi Satoshi-san,
Regards,
Anil.
Hi Anil-san,
I have one additional question regarding the boot flow.
In order to flash boot our existing AMP-based software, we found that some additional modifications were required beyond what is described in the provided PDF.
Specifically, by modifying the makefile_ccs_bootimage_gen, we were able to make the SBL recognize the A53 application as an SMP configuration.
Is this modification approach considered the recommended way?
Best regards,
Please refer to the attached file for the details of the differences. Due to file type restrictions, it is provided as a .txt file.
#
# Auto generated makefile
#
# Below variables need to be defined outside this file or via command line
# - MCU_PLUS_SDK_PATH
# - PROFILE
# - CG_TOOL_ROOT
# - OUTNAME
# - CCS_INSTALL_DIR
# - CCS_IDE_MODE
CCS_PATH=$(CCS_INSTALL_DIR)
include $(MCU_PLUS_SDK_PATH)/imports.mak
include $(MCU_PLUS_SDK_PATH)/devconfig/devconfig.mak
LD=$(CG_TOOL_ROOT)/bin/aarch64-none-elf-ld
STRIP=$(CG_TOOL_ROOT)/bin/aarch64-none-elf-strip
OBJCOPY=$(CG_TOOL_ROOT)/bin/aarch64-none-elf-objcopy
ifeq ($(OS), Windows_NT)
PYTHON=python
else
PYTHON=python3
endif
OUTFILE=$(PROFILE)/$(OUTNAME).out
BOOTIMAGE_PATH=$(abspath ${PROFILE})
BOOTIMAGE_NAME:=$(BOOTIMAGE_PATH)/$(OUTNAME).appimage
BOOTIMAGE_NAME_XIP:=$(BOOTIMAGE_PATH)/$(OUTNAME).appimage_xip
BOOTIMAGE_NAME_SIGNED:=$(BOOTIMAGE_PATH)/$(OUTNAME).appimage.signed
BOOTIMAGE_RPRC_NAME:=$(BOOTIMAGE_PATH)/$(OUTNAME).rprc
BOOTIMAGE_RPRC_NAME_XIP:=$(BOOTIMAGE_PATH)/$(OUTNAME).rprc_xip
BOOTIMAGE_RPRC_NAME_TMP:=$(BOOTIMAGE_PATH)/$(OUTNAME).rprc_tmp
#
# Generation of boot image which can be loaded by Secondary Boot Loader (SBL)
#
ifeq ($(OS),Windows_NT)
EXE_EXT=.exe
endif
ifeq ($(OS),Windows_NT)
BOOTIMAGE_CERT_GEN_CMD=powershell -executionpolicy unrestricted -command $(MCU_PLUS_SDK_PATH)/tools/boot/signing/x509CertificateGen.ps1
else
BOOTIMAGE_CERT_GEN_CMD=$(MCU_PLUS_SDK_PATH)/tools/boot/signing/x509CertificateGen.sh
endif
BOOTIMAGE_TEMP_OUT_FILE=$(PROFILE)/temp_stdout_$(PROFILE).txt
BOOTIMAGE_CORE_ID_a53ss0-0 = 0
BOOTIMAGE_CORE_ID_a53ss0-1 = 1
BOOTIMAGE_CORE_ID_a53ss1-0 = 2
BOOTIMAGE_CORE_ID_a53ss1-1 = 3
BOOTIMAGE_CORE_ID_r5fss0-0 = 4
BOOTIMAGE_CORE_ID_m4fss0-0 = 5
BOOTIMAGE_CORE_ID_hsm-m4fss0-0 = 6
BOOTIMAGE_CORE_ID_load_only = 21
SBL_RUN_ADDRESS=0x43C00000
SBL_DEV_ID=55
SW_VERSION=0x00000000
MULTI_CORE_IMAGE_GEN = $(CCS_NODE) $(MCU_PLUS_SDK_PATH)/tools/boot/multicoreImageGen/multicoreImageGen.js
OUTRPRC_CMD = $(CCS_NODE) $(MCU_PLUS_SDK_PATH)/tools/boot/out2rprc/elf2rprc.js
APP_IMAGE_SIGN_CMD = $(MCU_PLUS_SDK_PATH)/tools/boot/signing/appimage_x509_cert_gen.py
ifeq ($(OS),Windows_NT)
XIPGEN_CMD=$(MCU_PLUS_SDK_PATH)/tools/boot/xipGen/xipGen.exe
else
XIPGEN_CMD=$(MCU_PLUS_SDK_PATH)/tools/boot/xipGen/xipGen.out
endif
MULTI_CORE_IMAGE_PARAMS = \
$(BOOTIMAGE_RPRC_NAME)@$(BOOTIMAGE_CORE_ID_a53ss0-0) \
MULTI_CORE_IMAGE_PARAMS_XIP = \
$(BOOTIMAGE_RPRC_NAME_XIP)@$(BOOTIMAGE_CORE_ID_a53ss0-0) \
all:
ifeq ($(CCS_IDE_MODE),cloud)
# No post build steps
else
@echo Boot image: am62x:a53ss0-0:freertos:gcc-aarch64 $(BOOTIMAGE_NAME) ...
$(OUTRPRC_CMD) $(OUTFILE) $(SW_VERSION)>> $(BOOTIMAGE_TEMP_OUT_FILE)
$(COPY) $(OUTNAME).rprc $(BOOTIMAGE_RPRC_NAME)
$(COPY) $(BOOTIMAGE_RPRC_NAME) $(BOOTIMAGE_RPRC_NAME_TMP)
$(RM) $(BOOTIMAGE_RPRC_NAME)
$(XIPGEN_CMD) -i $(BOOTIMAGE_RPRC_NAME_TMP) -o $(BOOTIMAGE_RPRC_NAME) -x $(BOOTIMAGE_RPRC_NAME_XIP) --flash-start-addr 0x60000000 -v > $(BOOTIMAGE_TEMP_OUT_FILE)
$(MULTI_CORE_IMAGE_GEN) --devID $(SBL_DEV_ID) --out $(BOOTIMAGE_NAME) $(MULTI_CORE_IMAGE_PARAMS) >> $(BOOTIMAGE_TEMP_OUT_FILE)
$(MULTI_CORE_IMAGE_GEN) --devID $(SBL_DEV_ID) --out $(BOOTIMAGE_NAME_XIP) $(MULTI_CORE_IMAGE_PARAMS_XIP) >> $(BOOTIMAGE_TEMP_OUT_FILE)
# Sign the appimage for HS-FS using appimage signing script
$(PYTHON) $(APP_IMAGE_SIGN_CMD) --bin $(BOOTIMAGE_NAME) --authtype 0 --loadaddr 8A000000 --key $(APP_SIGNING_KEY) --output $(BOOTIMAGE_NAME).hs_fs --keyversion $(VERSION)
ifeq ($(DEVICE_TYPE),HS)
# Sign the appimage using appimage signing script
ifeq ($(ENC_ENABLED),no)
@echo Boot image signing: Encryption is disabled.
$(PYTHON) $(APP_IMAGE_SIGN_CMD) --bin $(BOOTIMAGE_NAME) --authtype 0 --loadaddr 8A000000 --key $(APP_SIGNING_KEY) --output $(BOOTIMAGE_NAME).hs --keyversion $(VERSION)
else
@echo Boot image signing: Encryption is enabled.
$(PYTHON) $(APP_IMAGE_SIGN_CMD) --bin $(BOOTIMAGE_NAME) --authtype 0 --loadaddr 8A000000 --key $(APP_SIGNING_KEY) --enc y --enckey $(APP_ENCRYPTION_KEY) --output $(BOOTIMAGE_NAME).hs --keyversion $(VERSION)
$(RM) $(BOOTIMAGE_NAME)-enc
endif
endif
$(RM) $(BOOTIMAGE_RPRC_NAME_TMP)
@echo Boot image: am62x:a53ss0-0:freertos:gcc-aarch64 $(BOOTIMAGE_NAME) Done !!!
@echo .
ifeq ($(DEVICE_TYPE),HS)
@echo Boot image: am62x:a53ss0-0:freertos:gcc-aarch64 $(BOOTIMAGE_NAME).hs Done !!!
@echo .
else
@echo Boot image: am62x:a53ss0-0:freertos:gcc-aarch64 $(BOOTIMAGE_NAME).hs_fs Done !!!
@echo .
endif
endif
#
# Auto generated makefile
#
# Below variables need to be defined outside this file or via command line
# - MCU_PLUS_SDK_PATH
# - PROFILE
# - CG_TOOL_ROOT
# - OUTNAME
# - CCS_INSTALL_DIR
# - CCS_IDE_MODE
CCS_PATH=$(CCS_INSTALL_DIR)
include $(MCU_PLUS_SDK_PATH)/imports.mak
include $(MCU_PLUS_SDK_PATH)/devconfig/devconfig.mak
LD=$(CG_TOOL_ROOT)/bin/aarch64-none-elf-ld
STRIP=$(CG_TOOL_ROOT)/bin/aarch64-none-elf-strip
OBJCOPY=$(CG_TOOL_ROOT)/bin/aarch64-none-elf-objcopy
ifeq ($(OS), Windows_NT)
PYTHON=python
else
PYTHON=python3
endif
OUTFILE=$(PROFILE)/$(OUTNAME).out
BOOTIMAGE_PATH=$(abspath ${PROFILE})
BOOTIMAGE_NAME:=$(BOOTIMAGE_PATH)/$(OUTNAME).appimage
BOOTIMAGE_NAME_XIP:=$(BOOTIMAGE_PATH)/$(OUTNAME).appimage_xip
BOOTIMAGE_NAME_SIGNED:=$(BOOTIMAGE_PATH)/$(OUTNAME).appimage.signed
BOOTIMAGE_RPRC_NAME:=$(BOOTIMAGE_PATH)/$(OUTNAME).rprc
BOOTIMAGE_RPRC_NAME_XIP:=$(BOOTIMAGE_PATH)/$(OUTNAME).rprc_xip
BOOTIMAGE_RPRC_NAME_TMP:=$(BOOTIMAGE_PATH)/$(OUTNAME).rprc_tmp
#
# Generation of boot image which can be loaded by Secondary Boot Loader (SBL)
#
ifeq ($(OS),Windows_NT)
EXE_EXT=.exe
endif
ifeq ($(OS),Windows_NT)
BOOTIMAGE_CERT_GEN_CMD=powershell -executionpolicy unrestricted -command $(MCU_PLUS_SDK_PATH)/tools/boot/signing/x509CertificateGen.ps1
else
BOOTIMAGE_CERT_GEN_CMD=$(MCU_PLUS_SDK_PATH)/tools/boot/signing/x509CertificateGen.sh
endif
BOOTIMAGE_TEMP_OUT_FILE=$(PROFILE)/temp_stdout_$(PROFILE).txt
BOOTIMAGE_CORE_ID_a53ss0-0 = 0
BOOTIMAGE_CORE_ID_a53ss0-1 = 1
BOOTIMAGE_CORE_ID_a53ss1-0 = 2
BOOTIMAGE_CORE_ID_a53ss1-1 = 3
BOOTIMAGE_CORE_ID_r5fss0-0 = 4
BOOTIMAGE_CORE_ID_m4fss0-0 = 5
BOOTIMAGE_CORE_ID_hsm-m4fss0-0 = 6
BOOTIMAGE_CORE_ID_load_only = 21
BOOTIMAGE_CORE_ID_freertos-smp = 100
SBL_RUN_ADDRESS=0x43C00000
SBL_DEV_ID=55
SW_VERSION=0x00000000
MULTI_CORE_IMAGE_GEN = $(CCS_NODE) $(MCU_PLUS_SDK_PATH)/tools/boot/multicoreImageGen/multicoreImageGen.js
OUTRPRC_CMD = $(CCS_NODE) $(MCU_PLUS_SDK_PATH)/tools/boot/out2rprc/elf2rprc.js
APP_IMAGE_SIGN_CMD = $(MCU_PLUS_SDK_PATH)/tools/boot/signing/appimage_x509_cert_gen.py
ifeq ($(OS),Windows_NT)
XIPGEN_CMD=$(MCU_PLUS_SDK_PATH)/tools/boot/xipGen/xipGen.exe
else
XIPGEN_CMD=$(MCU_PLUS_SDK_PATH)/tools/boot/xipGen/xipGen.out
endif
MULTI_CORE_IMAGE_PARAMS = \
$(BOOTIMAGE_RPRC_NAME)@$(BOOTIMAGE_CORE_ID_freertos-smp) \
MULTI_CORE_IMAGE_PARAMS_XIP = \
$(BOOTIMAGE_RPRC_NAME_XIP)@$(BOOTIMAGE_CORE_ID_freertos-smp) \
all:
ifeq ($(CCS_IDE_MODE),cloud)
# No post build steps
else
@echo Boot image: am62x:a53ss0-0:freertos-smp:gcc-aarch64 $(BOOTIMAGE_NAME) ...
$(OUTRPRC_CMD) $(OUTFILE) $(SW_VERSION)>> $(BOOTIMAGE_TEMP_OUT_FILE)
$(COPY) $(OUTNAME).rprc $(BOOTIMAGE_RPRC_NAME)
$(COPY) $(BOOTIMAGE_RPRC_NAME) $(BOOTIMAGE_RPRC_NAME_TMP)
$(RM) $(BOOTIMAGE_RPRC_NAME)
$(XIPGEN_CMD) -i $(BOOTIMAGE_RPRC_NAME_TMP) -o $(BOOTIMAGE_RPRC_NAME) -x $(BOOTIMAGE_RPRC_NAME_XIP) --flash-start-addr 0x60000000 -v > $(BOOTIMAGE_TEMP_OUT_FILE)
$(MULTI_CORE_IMAGE_GEN) --devID $(SBL_DEV_ID) --out $(BOOTIMAGE_NAME) $(MULTI_CORE_IMAGE_PARAMS) >> $(BOOTIMAGE_TEMP_OUT_FILE)
$(MULTI_CORE_IMAGE_GEN) --devID $(SBL_DEV_ID) --out $(BOOTIMAGE_NAME_XIP) $(MULTI_CORE_IMAGE_PARAMS_XIP) >> $(BOOTIMAGE_TEMP_OUT_FILE)
# Sign the appimage for HS-FS using appimage signing script
$(PYTHON) $(APP_IMAGE_SIGN_CMD) --bin $(BOOTIMAGE_NAME) --authtype 0 --loadaddr 8A000000 --key $(APP_SIGNING_KEY) --output $(BOOTIMAGE_NAME).hs_fs --keyversion $(VERSION)
ifeq ($(DEVICE_TYPE),HS)
# Sign the appimage using appimage signing script
ifeq ($(ENC_ENABLED),no)
@echo Boot image signing: Encryption is disabled.
$(PYTHON) $(APP_IMAGE_SIGN_CMD) --bin $(BOOTIMAGE_NAME) --authtype 0 --loadaddr 8A000000 --key $(APP_SIGNING_KEY) --output $(BOOTIMAGE_NAME).hs --keyversion $(VERSION)
else
@echo Boot image signing: Encryption is enabled.
$(PYTHON) $(APP_IMAGE_SIGN_CMD) --bin $(BOOTIMAGE_NAME) --authtype 0 --loadaddr 8A000000 --key $(APP_SIGNING_KEY) --enc y --enckey $(APP_ENCRYPTION_KEY) --output $(BOOTIMAGE_NAME).hs --keyversion $(VERSION)
$(RM) $(BOOTIMAGE_NAME)-enc
endif
endif
$(RM) $(BOOTIMAGE_RPRC_NAME_TMP)
@echo Boot image: am62x:a53ss0-0:freertos-smp:gcc-aarch64 $(BOOTIMAGE_NAME) Done !!!
@echo .
ifeq ($(DEVICE_TYPE),HS)
@echo Boot image: am62x:a53ss0-0:freertos-smp:gcc-aarch64 $(BOOTIMAGE_NAME).hs Done !!!
@echo .
else
@echo Boot image: am62x:a53ss0-0:freertos-smp:gcc-aarch64 $(BOOTIMAGE_NAME).hs_fs Done !!!
@echo .
endif
endif
Hi Satoshi-san,
I am routing your query to Boot expert to comment on the above your queries .
Regards,
Anil.
Is this modification approach considered the recommended way?
Or is there a more appropriate or standard method to handle SMP boot image generation on A53?
These modifications are required for SMP to work, We generally recommend using any SMP example provided in the SDK like hello world as a base and modify it to create your custom application.
Hi Meet-san,
Understood. Thank you for the clarification.
We'll proceed with this approach.
Best regards,
Satoshi
Hi,
This bottleneck seems to be due to all A53 cores sharing a single L2 cache and is expected. All cores directly compete for the same L2 cache space, When Core1-Core3 are idle, Core0 has near-exclusive L2 access for your audio workload once you overload all cores this becomes an issue with all cores accessing the same L2 cache space, this may also lead to DDR Memory Bandwidth contention because L2 misses go directly to DDR.
Best Regards,
Meet.