This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM2912A: temperature range and cold start

Part Number: PCM2912A

The specification of the part under abslute maximum ratings section,  states low ambient temperature of -40 Deg C. But the operating free air low temperature is -25 Deg C. So does the component supports -40 Deg C cold start? is it allowed for normal operaion. does the low temperature demand is because of reduced performance, or is it required because of MTBF issue.

Thanks, 

Adi

  • Hi Adi,

    There is risk of reduced performance outside of Recommended Operating Conditions. So for normal operation, I recommend above -25C. Below this, the part will not be damaged, but reduced performance is likely. There is risk of permanent damage below -40C operating temperature.

    Best,

    Garret