Part Number: TAS5782M
Hello,
Our customer is facing on a critical issue in TAS5782M 3 wire interface configuration following to the e2e thread below.
Then he has some questions about system clock and LRCK/FS relationship changes more than +/-5 MCLK case that is described in the datasheet "9.3.3.5 Serial Audio Port - Data Formats and Bit Depths" in below.
If the relationship between LRCK/FS and system clock changes more than ±5 MCLK, internal operation is initialized within one sample period and analog outputs are forced to the bipolar zero level until resynchronization between LRCK/FS and system clock is completed.
Q-1 : How does the customer set the "system clocks" wretten in bold ?
Q-2 : Is this function able to disable by resister bit ?
Best regards,