TLV320AIC3105: Questions regarding the datasheet

Part Number: TLV320AIC3105
Other Parts Discussed in Thread: TLV320AIC3104

Hi team,

Could you please check the datasheet for the TLV320AIC3105, as there are some sections that are unclear?
-On page 22, in section 10.3.3 Audio Data Converters, does “NCODEC = NDAC = NDAC” in the text mean “NCODEC = NDAC = NADC”?
-On page 52, the description for Table 21. Page 0/Register 15 says “Left-ADC,” but should this be “Right-ADC”?
-On page 69, the DESCRIPTION for Table 66. Page 0/Register 60, Table 68. Page 0/Register 62, and Table 69. Page 0/Register 63 is unreadable. The BIT fields also appear to have D7 and D6-0 grouped together when compared with similar registers, so I would like to know the correct tables and descriptions.

Also, if these are errors, are there any plans to correct them?
Is there a block diagram available for the TLV320AIC3104 (a variant with different functionality), similar to the one on page 21, that shows the associated register assignments on the diagram?
 
Best Regards,
Ryu.