Other Parts Discussed in Thread: PCM3070
Anyone able to use this module with the USB-MODEVM interface board?
I've sent back two already, neither one works properly. Patrick in "tech support" isn't able to offer any help. Thought I check and see if this is a Me thing, or a bad EVM implementation.
Here's the story:
- I can communicate with the 3070 via the PCM3070-K CS software no problem.
- I can turn blocks on and off, get register information, flag information... all good.
- I can route Analog audio from the line input to the line or headphone output via the "analog bypass"
- I can adjust levels in the amplifier no problem. All in analog bypass.
- What it won't do is pass any audio from the A/D to D/A and out.
- Won't take any Digital audio from the USB connection to the D/A and out. None.
- None of the apps in the PCM3070EBM-K software work.
PCM3070-K CS Version 1.2.3
USB-MiniEVM ver. 2.03
Anyone able to get this to work?