PCM5100A: PCM5100AQPWRQ1- LDOO Value

Part Number: PCM5100A

Hi Team,

For PCM5100AQPWRQ1, I need the LDOO minimum and maximum voltage values for analysis. I am unable to locate these values in the datasheet.

  • Hello Jishna,

    Since this is an  internal LDO and used by the internal modules, no specs are provided, only the compensation caps are external and seen by the external world.

    So we can not provide a min or max for internal LDO. However, it should not vary more than  3% at most.

    Regards,

    Arash