DIX9211: Using the DIX9211 for high sample rates in combination with I2S in bypass mode

Part Number: DIX9211

Hello,
I am currently building a DA converter for a client which, in addition to a USB audio input, is to feature two SPDIF inputs and one AES3 input.
I would like to use a DIX9211PT as the receiver for the two SPDIF inputs and the AES3 input.
The MCU that converts the USB audio data stream to I2S supports data rates from 44.1 kHz to 786 kHz (PCM) and DSD 64, 128, 256 and 512.
To avoid using additional ICs to route this I2S/DSD section, I would like to route these signals via the DIX9211PT (I2S interface).
My question is: can the DIX9211PT handle these high data rates or sample rates in bypass mode?

Thanks