This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

2 masters on the same clock

Other Parts Discussed in Thread: CC8531

Hello,

I would like to know if it is possible to connect 2 masters on the same clock so their using the CC8531 headset device ?

Thanks

Hugo

  • Hi Hugo, 

    Two devices can indeed be clock sourced externally from the same source. You select this in the audio interface panel of the PurePath Wireless configurator (clock source can be external, internal with MCLK or internal without MCLK). 

    From the other questions you have posted I'm not sure if I have grasped the real meaning behind your questions nor understand the application scenario you are trying to solve. 
    If you can clarify it will increase the chance of us providing you a good answer.

    Best regards,
    Kjetil