Part Number: SRC4382
Hi ti team,
The new project is using the SRC4382. Please help check if there are any issues with the attached schematic. Thanks

Hi,
Here are few suggestions:
1- I would add 22-100 Ohm series resistors to the I2S lines.
2- I would use about up to 10uF and 100nF parallel caps to GND on all supply lines including VIO.
3- I don't think adding series resistors to all digital input pins is needed, internally they have protection ( such as ESD) .
4- LOCK is output flag, remove the resistor
5- use pull up resistors to IOVDD for I2C pins
Kind Regards,
Arash