Part Number: PUREPATHSTUDIO
Other Parts Discussed in Thread: TAS2781
I'm using PPC3 version

After creating the tuning and audio processing of my choice, I go to End System Integration and generate the CFG, headers and binary files.
I then go back to the end system integration and select Verify Binary File. The result is below.

Generated CFG and binary files.
Please help replicate on your system to make sure what I am doing is correct.
When I load the generated CFG file back into the EVK after a power cycle. The speaker is outputing loud noises, as if the sampling frequencies are off.
When I load the PPC3 file configuration via the Tuning and Audio Processing or Device Control, the speaker behaves like the tuning I created.
I then used the I2C monitor feature to record the data sent to the TAS2781 via the Tuning and Audio Processing vs the generated CFG file and they are different. If I use the I2C monitor capture and save it as a CFG and load that via the Direct I2C tool, then everything works as expected. The generated CFG always fails to load properly.
All these tests are done on the TI TAS2781 EVM.