Other Parts Discussed in Thread: TLV320AIC3254, PUREPATHSTUDIO
Hello.
We are designing a SSB receiver using the Weaver method with the
TLV320AIC3254 part. Our system relies greatly on properties of the ADC
decimation fiters and the decimation filter A seems to fit the bill
for us with sampling frequency of 44100 sampels per second. We would
greatly benefit from being able to implement further low pass
filtering & decimation on the miniDSP as the SSB channel is only 3kHz
wide and centered around zero frequency. Therefore further 4x
decimation will improve system noise and lower current consumption. Is
there a way to implement multirate processing on the miniDSP with
PurePathStudio? Is there a way to insert a 2nd decimation block into
PPS? Could an additional low pass filtering & decimation block be
provided to further versions of PPS?
We would also like to utilize the ADC preamp and DRC blocks to
implement automatic volume control for the radio. While the two blocks
work well on their own, they don't know about each other's action. We
would like to control the two synchronously. Is there a way to control
the ADC preamp gain from the miniDSP programatically apart from the
standard AGC block?
Thanks, Ondra