Other Parts Discussed in Thread: TAS5630, TAS5630B
Hello experts,
I am developing an amplifier in 2.1 system application by using TAS5630 IC. Everything works fine except the strange trouble of channel separations.
My configurations of TAS5630 amp:
-- Channel A & B are working in BTL mode, as subwoofer amplifier
-- Channel C & D are working in SE mode, as satellites
Problem description:
-- Sin wave signal applies to subwoofer channel, no audio signal to satellites, but satellites amp have very annoying audiable noise. Noise keeps there even no speaker load connected to subwoofer (means keep subwoofer amp open)
-- Noise frequency from satellites changes when sin-wave input signal's amplitude changes, very strange
Eforts tried:
1) I thought noise might come from the pre-amp stage, possibly bad ground loop or what ever. I did a test to cut out the pre-stage of Channel C & D, connect input (before DC block capacitor) directly to AGND. It does not help, problem still there
2) Can output stage involve noise in? I did a test by even removing the output filter of Channel A&B completely, means channel A&B are working (I do see the outA & outB signals) but no current out. It does not help, problem still there
3)Too much noise at AGND pin? I connect even this pin directly to audio gnd with an additional wires, no help.
4) Can 12V auxilary power supply cause the problem? I solder out the on-board 12V auxilary power supply block, and connect by an additional power source (followed by a 7812 regulator). No help
Additional information
A) I reconfigure the system to stereo application, means Channel A&B in BTL mode, and Channel C&D in BTL mode. Surprised to see that there is no problem any more, means 2 channels work independently well.
B) I did another further test in stereo application, I connect 2pcs 2-Ohm speakers in series as load of Channel C & D, and connect the junction of 2 speakers to 1/2PVCC of channel C & D (you can call this as a similar 2pcs SE amp). Idea behind was to see whether the problem is still there, but just compensated each other between Channel C & D. Result showed that both speakers noisy. (cut the connection between mid of 2 speakers & 1/2PVCC of Channel C&D, problem disappear)
Does any of you meet this problem?
Junpu