Other Parts Discussed in Thread: TAS5631
Hello,
I'm student. My School bought a TAS5631DKD2EVM with Input-USB Board 2 and it was given to me as project to understand how it works and make a documentation of them together in french, but I don't really understand how it works.
I tried to do a first test with an oscillator instead of loudspeaker, but I got nothing. I supplied the Input-USB Board 2 with 15V and I put a song in the analog input SDIN1 (CH 1+2). I supplied the TAS5631DKD2EVM only with 35 V (20 - 50V recommended) and I put an oscillator instead of loudspeaker. I did some configurations in the GUI also and unmuted the Input-USB Board 2. my first question is, does it work like that? should I also supply the TAS5631DKD2EVM with 12V for regulators?
Here the configurations I did:
- mode BTL
- master volume : +15
- Fs = 48kHz
- bass & treble inline (on)
- Loudness filter file : Loudness2_48k
- Loudness gain : 1.0000
- Compression : DRC1, pre-volume DRC
- DRC parameter file : late_night48.drc550x
Second question: how should I configurate the GUI for a first test?
Third: as input of the Input-USB Board 2, i only put a song through analog input. is that ok?
And last question: what should I do step by step to perform a first test of both Input-USB Board 2 and TAS5631DKD2EVM?
Sorry for my bad English. I hope you will understand my questions and find how to help me.
Thanks.