Hello All,
I inherited an old design that I’m looking to update. One of the things that I would like to update is an amplification circuit. Currently they are using an LM4951SD, as the heart of the circuit. They have a 60kHz square wave being turned into a 60kHz sine wave via a Capacitor Inductor Filter Circuit. Then it goes to a digi-pot for its first amplification then to the LM4951SD, where the VO+ is left floating and the VO- goes to an auto transformer and then out of the device.
It’s basically straight up amplification of a sine wave that’s made up of a 3 stage circuit, the audio amp they are using is limited, and I know there are newer ones out there, and it’s not like we are using it all to rigorously so I was hoping I could find some simple alternatives and end up removing some of the circuit. Ideally I’d like to keep it to a single amplification stage but I need a higher power amp. Any help would be appreciated, thank you for your time.