Hi,
I'm trying to use the LM49352 in Master mode (generates the clock and sync to my I2S interface). From the documentation, it is not obvious how the port clocks and the converter clocks are related (or have to be configured). Is there an app note on this? Or some example?
For example:
I have a 6.144MHz Mclk, and I want an 8K sample rate, then I generate the clock for the DAC to be 2.048MHz (2*OSR*Fs). Fine per document.
Now what should be the Port clock frequency?
I would expect the port output clock (master mode) to generate a frequency of 32*fs (for 16-bit samples of L/R channels). Does the port operating frequency = this or is it higher, or do I have apply interpolation,
Any help would be appreciated.
Thanks,
Gary