I've been using the PPWC program for over a year on a project. I've just recently upgraded to version 1.3.0.36447 and created a new custom project. My quandary, when I select the Custom design option for the Hardware platform, I do not get the Audio Device Customization listing on the left configuration panel. I've imported older projects (version 1.2.2) and the Audio Device Customization item is shown. I've even tried adding the custom code from the older project and it still doesn't show up. What I'm trying to do is create a master with two mono mic slaves.
Anyone have thoughts on what could be happening?