Other Parts Discussed in Thread: TAS5630
hello,
I have a customer that has a doubt about the frequency response of the TAS5630 at the following application: single-ended (SE), 2 ohm load.
Currently they have a good frequency responce of 70 Hz to over 20 KHz [board mounted with TAS5630] and they would like to work with lower frequency signals like 40 Hz, it means that the amplifier must have a bandwidth greater than the current one, the limit bottom of the bandwith should be changed from the current 70 Hz to 40 Hz. What could be done to improve the low frequency response?
thanks,
Bruno Nunes