Hi All,
this is my problem: I have a master with the firmware "Audio Input Bi-directional Master", and a slave host controlled (Headset Kit). Setting the NWM_ACH_SET_USAGE {0x00 0x01 0xFF..}, the slave receive the audio from the master and there's no trasmission from slave to master.
Setting 0x01 on position "Microphone 1" there's no trasmission from slave to master again.
Where is the error?
(Firmware - Audio streaming of the slave device:
master to slave: AD1 left 0, AD1 right 1
slave to master:AD0 Left 0)
Thanks!
Francesco