Hi,
Occasionally when the LM48511 Class-D audio amp starts up there is no output from the H-Bridge. The boost converter still works and the analog amp still works but the output on LS+ and LS- is low. This seems to occur when there is a break in the power supply. If the supply to VDD slowly drops to ~0.3-1V and the power is then restored the H-Bridge appears to lock up. I can reduce the likelihood of this happening by loading the VDD supply so it falls quickly.
Is it possible to stop this from happening?