Other Parts Discussed in Thread: CC8530
Hi all,
my question is this:
is it possible make a network (using headsetEM) with one master and 3 or 4 slave with the a bidirectional communication between master and slave?
I understand that the cc8530 has a maximun number of 4 channel but it needs an AIC34 codec and on the headset board there is a AIC3204 codec (2 channel); there's no application role in the Purepath configurator similar to this configuration..
Using instead the "dual headset base station" application role, is it possible make the network with one master and 2 slave (bidirectional master-slave)?
if I set the slave's audio channel setup slave-to-master -> channel right for a slave and channel left for the other one, it should work, right?
Thanks
Best regards
Francesco