Other Parts Discussed in Thread: LM4667, LM4671
I am using an LM4667 in an application which drives the LM4667 in single ended mode with the -ve input AC coupled to an opamp drive and the +ve input AC coupled to ground, as per one of the suggested configurations in the datasheet. I'm finding that there is a low level whistling/rasping noise when the amp is idling with no audio input which doesn't seem to be relating to supply decoupling (operating at 5V) and there doesn't seem to be any instability in the driving audio chain. If I DC couple the +ve input, the noise goes away but there's then a large speaker click when the speaker enable input is changed. If I DC couple both inputs, the speaker click goes away but a constant low level whistle is present (maybe about 10kHz). Has anyone experienced these sorts of issues with the LM4667?