Hi,
This is not immediately obvious but it seem we cannot use the PRB_P & PRB_R (DAC & ADC Signal Processing Blocks) at the same time as the miniDSP ?!?
I have been using the AIC3204 with some basic biquad filters and would like to keep them on the AIC3254 whilst also using the miniDSP for noise reduction etc. Is this possible or can I only use the miniDSP without the PRBs for instance ? I have also been using the BEEP generator so a particular PRB_P had to be configured to generate the BEEP. How do I generate a BEEP whilst using the miniDSP on the AIC3254 at the same time ?
regards, M