Other Parts Discussed in Thread: PCM2906C
Hello: my customer has a question on the PCM2906 USB codec:
>>>>
The application is for a PTT headset with two sources of audio inputs to the earphones, one to the right and the other to the left. One audio source is analog audio from a Smartphone, and the other is a digital source from a radio, through the radio's USB port.
The PTT needs to be powered from either the USB port or from the smartphone side (only when the radio is not connected).
A question from the end customer that needs answer immediately is "can the PCM2906C operate independently, passing the analog audio from the smartphone to the PTT's earphone, without the USB port being connected?"
Can you help or direct to someone familiar with this PCM2906C?
Currently, another end customer is designing this PTT, but the Codec used in the design is NXP UDA1325, which may be obsolete already, so we should be able to get PCM2906C into the design.
>>>>
I think this will require an AIC32xx codec and a separate streaming USB device. Also, not sure of which codec can do independent right and left signals (most are dedicated stereo). Please advise on the best way to do this, thanks.
George Biner