Did have TI some future plans about creating USB DAC or CODEC with USB audio class 2.0 support for 96kHz and 192kHz/24bit sample frequency? I like simple chips like PCM2706 DAC with I2S support or PCM2902 CODEC. There exists some chips from Tenor or XMOS and M2Tech but they are too complicated and access to documentation is not much good. I like TI chips, but I want to create USB soundcard with I2S output for my PCM1704 based HiFi DAC.