Hello,
I am using the cc8531DK Headset to transmit data. But as i would like to transmit 4 audio channels in PCM (16 or 24), i have to use 2 master cards and 2 slave cards. I would like to synchronize the 2 masters so the signals i receive on the slaves are synchronized too.
My problem is that i am trying to give the master cards an external clock, but when i pair the cards together, they put themselves in a standby mode.
To be able to configure the cards this way in the purepath wireless configurator, i have modified the codec file so i can activate this external clock. I have tried to input this external clock on all the clock pins (MCLK, BCLK, WCLK) but nothing change.
Where should i input my external clock so it works ?
Thanks for your answer.
Hugo