This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

using an I2S source without MCLK for TAS5508C

Other Parts Discussed in Thread: TAS5508C, TLV320AIC3206

Hi All,

  We are working on a 2.1 channel audio amp with TAS5508C.  (It is a long story on why we use an 8-channel controller for 2.1 design.)  There are several audio sources: I2S out from LM3S9B96 and an BT module.

  LM3S9B96 provides its own master MCLK and I2S data so we are fine here.  However, the BT module is a master I2S but it only provides SCK, WS (Word Select) & SD (Serial Data).  It doesn't provide any MCLK signal.  BTW, the BT module uses 48K hz sample rate.

  Here are my questions:

  1. Is there any way to interface this BT module directly to TAS5508C?

  2. If that is an option, I am thinking to use BT I2S as input to LM3S9B96 and let LM3S9B96 output the audio data to its I2S output port along with MCLK.  It seems to be a possible solution but we need to write some code in LM3S9B96.   Has anyone had this successfully?  Or does anyone have any comment/suggestion?