This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM4780 Ground connection



I am wanting to hook up the LM4780 in a parallel configuration and have been talking in the past to Royce Higashi who has been very helpful. In any event, do the ground -pins ( 12 and 19)- hook up to the floating dual polarity supply ground or is it a separate ground of some type?

My calculation from the nomogram of supply voltage vs output power , page ten of the ap note, with a 4 ohm load,- for a single amplifier,- is about somewhere around 50 watts. That to me gives an output voltage, peak I suppose, of ( P * Load resistance) ^1/2 = ( 200) ^1/2 = 14 volts; peak I is then 14/4 amps = 3.5 amps. If that current, peak I, is flowing through the figure 3. Rout of 0 .1 ohm, then the wattage I need for Rout is about  I^2*R = 1 watt.

My other question is , with the single amp nomogram, of wattage versus voltage, when the amps are connected in parallel, is the output power doubled to 100 watts?

and would that change the calculations I need for the supply current?

 

 

  • Neil,

    The GND pins needs to be tied to a potential that is the mid point of the split supply.  For example, if you were using the Agilent E3631A power supply, you would connect the GND pins to the COM of the +/-25V output.  This ensures that the internal biasing is such that you get the maximum head room through the device. 

    For the Rout power, your calcuations are correct, but I would recommend giving yourself a little headroom and choose a 1.5-2W resistor. 

    The parallel configuration does not increase the voltage headroom, but it increases the current headroom.  Output power for single vs parallel will depend on your load impedance.  If you use the same load and supply voltage in both cases, your output power will not increase (assuming no current constraints).  With the same load impedance, your supply current will increase slightly, since you have two amplfiers driving the load.  But the load current will be the same as a single amp.

    If you change your load,  from 4ohms to 2ohms, then you will get an increase in power, as the parallel amplifier can provide double the current of the single amp.  The supply current will increase, as the parallel amps will drive more current..

     

    Regards,

    royce