This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSD1793 Audio DAC - Preferred Part?

Other Parts Discussed in Thread: DSD1793, PCM1792, PCM1796, PCM5122

We used the DSD1793 in a design a few years ago and it has worked well.  We are now designing an upgrade to the product and are planning on using the same device.  However, the DSD1793 isn't listed in the Q1 2012 Audio Guide, nor does it show up via the web Audio Selection Tool.  The product page says that it is still active.  Is there another part that is recommended for use in place of the DSD1793.  Basic requirements are: stereo DAC, SW control, 113dB min SNR, 96kHz min sample rate.

Thanks