Hi,
I have a question about simultaneous and synchronised wireless audio transmission to multiple devices.
I'm involved in a research project examining the effect of physical separation on music ensemble interaction and timing. Basically, I'm investigating how physically separating musicians from each other affects how they play 'together'.
To accomplish this, I need a high-quality wireless audio solution with minimal lag and the possibility to connect a single audio playback source to a large number (anywhere from 5 to 50+) of devices (e.g., headphones). Note that I want to transmit a single audio stream to multiple listeners (all listeners should be able to hear the same audio stream as synchronously as possible).
PurePath looks like an interesting technology, but, if I understand correctly, is limited to the transmission of only 4 simultaneous streams. Is this correct? If so, are there any alternative technologies available which can allow more listeners to simultaneously hear the same audio?
Many thanks in advance!
Geoff