Hello,
I have a customer using the CC8520 connected to 2 speakers and is having some problems with latency and seeing a 90ms delay between sending a datagram paket to the 1st speaker then another to the second speaker. Here are some questions they need answered.
1) does the purepath side-channel have expected times to send data (maybe avg and worst case)
2) If I were to send back-to-back data from one to another, how much latency should I expect between the two “packets”
3) if I send in one direction and then in the other, are there built in turn-around latencies that I need to take into account.
Thanks,
Rachel