Other Parts Discussed in Thread: TLV320AIC3204
I have referred SLAA446 Application Report entitled "Using the AGC, DRC and Beep Generator Function in TLV320AIC3204/54/3100/10/11/20/36 Devices", however, the effect of AGC has some problems as follows.
1. We set up Target Level (P0.R86) as a fixed value when input fixed volume, also to modify value of noise threshold (P0.R87) and to read Gain Applied (P0.R93) which is fixed and no full, in such situation, WHY output volume is also changed?
2. To read (P0, R45, D6), from has sound to no sound, we have read Fg =1 once, Fg=0 after first time. We try this experiment again, thus fg still is "1", For such result, we cannot sure the sound is input, how to make sure have sound IN, also what is purpose of Fg?
3. We can not meet effect of AGC like Figure 1 AGC function when finishing AGC setting.
4. What is the goal of DRC, We follow thr application note to set up related value for DRC, however, we can not face any effects about DRC.
5. We modified (P0.R83), Sometimes has some effects, but sometimes not any effects. Also, we set "+"db value but the sound is decreased, set "-"db value the sound is increased. Also, we read (P0,R93), however, (P0, R93) value has not any change. For such situation, is it correct working? Could you tell us how to solve above problems, thank you very much!