Is it OK to tie VcomR and VcomL (pins 22,21) together and use a common decoupling capacitor when using the PCM1792A in Mono mode? Also I am planning to use a pair of IV converters so I want to sum the current outputs IoutR+/IoutL- and IoutR-/IoutL+ and just want to see if there are any concerns around this. Also note that the diagram in Figure 39 of mono mode connection appears to have Out+ and Out- labeled incorrectly.