Hello,
I am testing my prototype of wireless speakers and after datagrams efficiency [:)] I am now fighting to optimize maximum range. I am rather unhappy with what I have now – less than 6 meters in the building when there are two or even one brick wall (14 cm thick) in between or 10 - 15 m outside – in the open air. That will not allow me to build a multizone hi-fi set that I am aiming at. I am using the evaluation kit PCB-s, a master is a PCB with a transceiver CC2590, and there are two speakers (slaves).
For now for the sake of optimization I have set the following:
Audio Streaming, 44,1 kHz, Audio Latency – 2048= 46 ms (max)
It improved the range a little (to the values quoted above) which seems weakish.
Are there any more things I can try to extend the range ? - setup options, hardware (different antenna ?)
What is the confirmed experience from the users ?
Regards, Pawel